GN 256 Silicone Vibration/Shock Absorption Mounts, Conical Type, Now Available from JW Winco

GN 256 Silicone Vibration/Shock Absorption Mounts, are frequently used as end-stop bumpers and can also be used as leveling feet. The silicone rubber material is age-resistant and has an increased working temperature range.

JW Winco, Inc., A Ganter Company, a leading supplier of standard industrial machine components, now offers GN 256 Silicone Vibration/Shock Absorption Mounts, Conical Type, with Stainless Steel Components.

Available with either a Tapped Hole or Threaded Stud, the RoHS compliant mounts are frequently used as end-stop bumpers and can also be used as leveling feet. The silicone rubber material is age-resistant and has an increased working temperature range.

Due to the material purity, it is possible to use the mounts in the food and medical industry. Absorbing most of the accumulated kinetic energy on impact, they act as dampers and prevent damaging shock and rebound. They also serve as sound dampers.

JW Winco offers an extensive selection of inch and metric size adjustable levers, cabinet U-handles, plastic and steel hinges and locking mechanisms, revolving and retractable handles, hand wheels, hand cranks, tube connection and conveyor components, inch and metric construction tubing, shock absorption mounts, leveling mounts, hand knobs, spring, ball and indexing plungers, jig, fixture and fastening components, retaining magnet assemblies, toggle clamps, metric casters and wheels, universal joints, oil sight glasses, and metric tools for the industrial and commercial equipment industries. JW Winco’s new website, with improved 3D CAD and online buying, is viewable at www.jwwinco.com.

      JW Winco, which is ISO 9001:2008 certified, is located in New Berlin, Wisconsin, with sales locations in Canada and Mexico. For more information, contact JW Winco at 800-877-8351, by fax at 800-472-0670, on the Web at www.jwwinco.com, and via e-mail at sales@jwwinco.com.

Back

JW Winco Press Releases

Click below for press releases on new products or additions and extensions to our product range!

Go to the Press Releases

New Products

Click below to hear about our new products or new additions to our product range!

Go to New Products