JW Winco Announces Availability of Steel and Stainless Steel Flat Knurled Thumb Screws

GN 653.2 Steel & Stainless Steel Flat Knurled Thumb

GN 653.2 Steel & Stainless Steel Flat Knurled Thumb Screws can be used to prevent loss of the thumb screw, due to the recessed portion of the stud

JW Winco, Inc., A Ganter Company, a leading supplier of standard industrial machine components, announced the offering of GN 653.2 Steel & Stainless Steel Flat Knurled Thumb Screws with Recessed Stud for Loss Protection.

The thumb screws, which are RoHS compliant, can be used to prevent loss of the thumb screw, due to the recessed portion of the stud. When using, instead of a typical tapped and bored hole, it is necessary to provide tapped bores with a thread on each of the two elements to be assembled. Additionally, a clearance bore on one or both sides is required.

Depending on the design and required clamping length of the component being attached, there are a number of assembly options. The steel knurled thumb screw body with a black oxide finish has tensile strength of class 5 and the visible face is fine turned. The stainless steel version is made of 303 stainless steel and comes with a matte, shot-blasted finish.

      JW Winco offers an extensive selection of inch and metric size adjustable levers, cabinet U-handles, plastic and steel hinges and locking mechanisms, revolving and retractable handles, hand wheels, hand cranks, tube connection and conveyor components, inch and metric construction tubing, shock absorption mounts, leveling mounts, hand knobs, spring, ball and indexing plungers, jig, fixture and fastening components, retaining magnet assemblies, toggle clamps, metric casters and wheels, universal joints, oil sight glasses, and metric tools for the industrial and commercial equipment industries. JW Winco’s new website, with improved 3D CAD and online buying, is viewable at www.jwwinco.com.

            JW Winco, which is ISO 9001:2008 certified, is located in New Berlin, Wisconsin, with sales locations in Canada and Mexico. For more information, contact JW Winco at 800-877-8351, by fax at 800-472-0670, on the Web at www.jwwinco.com, and via e-mail at sales@jwwinco.com

Back

JW Winco Press Releases

Click below for press releases on new products or additions and extensions to our product range!

Go to the Press Releases

New Products

Click below to hear about our new products or new additions to our product range!

Go to New Products