JW Winco at NAB

nab-jwwinco

JW Winco is exhibiting at the NAB show booth C12133!

JW Winco will be showing off our expanded range of inch and metric standard parts, offered in plastic, steel, stainless steel, cast iron and aluminum. In the Central Hall - Acquisition & Production area of the Las Vegas Convention center you will find JW Winco along with companies in the cameras and lenses, capture accessories, devices and software, lighting and grip, microphones, mobile/vehicle production, motion capture/virtual production, motion picture/film production, and set design/props/furniture and fixtures industries. JW Winco has been supplying these industries with levers, knobs, handles, handwheels, hinges, leveling feet and other components for a wide range of industrial applications.

New and featured JW Winco products on display at NAB!

  • GN 784 Mounting Clamps with Swivel Ball Joint can be used for mounting professional cameras, lights, monitors and stage gear that require quick adjustments.  Our GN 51.3 retaining magnets pair with the clamps for quick setup and mobility.
  • WN 100.1 T-handle rapid release pins have a wide range of applications in fastening, locating, and alignment applications. The WN 100.1 pins also can work for JBL replacement pins.
  • Telescopic slides are used in production facilities, mobile vehicles, Utility carts and economical sliding shelves with a variety of mounting options. They include partial, full, and over extension slides.
  • Adjustable levers have proven to be ideal for any application where frequent clamping or adjustments are made in a confined space or where the lever needs to be placed in a particular position.
  • Casters and wheels in different materials and sizes that can handle heavy loads for moving equipment or for rolling a cart.
  • Leveling devices to level a stage or equipment bases.
  • Handles and knobs in a variety of materials and sizes for any tensioning or clamping operation applications.

You can find JW Winco in booth C12133 in the Acquisition and Production area of the Central Hall! Stop in to see all of the different products JW Winco can provide!
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
Für diese Landesversion verlassen Sie die aktuelle Webseite und werden zur jeweiligen Landesvertretung weitergeleitet. Bitte beachten Sie, dass es zu Abweichungen von Darstellung und Inhalten kommen kann.

Sie werden nicht automatisch weitergeleitet. Bitte klicken Sie den unten genannten Link.

Note about forwarding

For this country version you leave the current website and are forwarded to the respective country representation. Please note that there may be deviations in presentation and content.