JW Winco Introduces Inch Set Screws Steel, With Brass or Nylon Tip

Set-Screws

New Inch Size Steel Set Screws, with Brass or Nylon Tip.

JW Winco, Inc., A Ganter Company, a leading supplier of standard industrial machine components, has recently introduced WN-913.3 Inch Size Steel Set Screws, with Brass or Nylon Tip.

      These set screws, with a black oxide finish, are used primarily in applications where you want to avoid the marring of a shaft or damaging a soft piece of material, but still need to secure it in place with the brass or nylon tipped set screw. They can be used with a variety of different parts, including levers, hand knobs, star knobs, and knurled nuts.

      “Those that operate in the area of machine building, including medical, packaging, and pharmaceutical, and material machining would find these set screws work very well for applications within these industries,” said John Winkler, CEO, Office of the President at JW Winco.

For the Metric set screws see the GN 913.3.
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
Für diese Landesversion verlassen Sie die aktuelle Webseite und werden zur jeweiligen Landesvertretung weitergeleitet. Bitte beachten Sie, dass es zu Abweichungen von Darstellung und Inhalten kommen kann.

Sie werden nicht automatisch weitergeleitet. Bitte klicken Sie den unten genannten Link.

Note about forwarding

For this country version you leave the current website and are forwarded to the respective country representation. Please note that there may be deviations in presentation and content.