JW Winco is exhibiting at the 2019 WestPack Show!

Westpack-Winco-components

WestPack is co-located with Medical Design & Manufacturing (MD&M) West, Automation Technology Expo (ATX) West, Design & Manufacturing Pacific, and Plastec West.

Leveling Devices, Adjusting Levers, Knobs, Anti Vibration Mounts, Indexing Plungers and other Components are used on the majority of the machines in the Packaging, Medical and Automation industry. JW Winco is a leader for manufacturing and supplying standard components for each of these industries.

In the packaging industry JW Winco supplies many Crank Handles, Hand wheels, Adjustable Levers and knobs for finishing machines and making accurate adjustments when needed. JW Winco’s GN 471.3 crank handle, VRAF spoked handwheel and GN / WN 300.1 adjustable lever are our top products for packaging machines. Packaging machines vibrate a lot and our GN 451 Vibration Isolation Mounts help reduce the wear on the machines. Our GN 342.2 Steel Vibration Damping Mounts help reduce noise and keep the machine steady.

Food packaging, increased food safety and sanitary guidelines for food (dairy, meat and poultry) producers/processors, and ready-to-eat food manufacturers must ensure their processing equipment meets the highest levels of hygiene and safety. JW Winco offers a Stainless Steel Hygienic Design product line that meets the high requirements of the EHEDG and the 3-A Sanitary Standards.

The medical industry in an important industry for JW Winco and our Stainless-Steel products along with our Hygienic Design products provide perfect solutions for medical manufactures. Our GN 822.9 mini indexing plunger is a top selling item along with the GN 617 stainless steel indexing plunger. Other top items for medical manufacturers are the GN 115.6 Mini-Latches Stainless Steel.

Automation uses a lot of JW Winco’s knobs, handles, vibration isolation mounts and leveling feet. JW Winco top leveling feet for automation are the WN 9000.1 leveling feet. Automation machines need stable environments, so nothing gets offset. Our GN 333.1 Tubular Handles are used on doors and frames of automation machines along with multiple hinges, like our GN 237 Zinc Die-Cast Hinges, that allow for easy access to the machines.   

Along with providing great application solutions for these industries, JW Winco also has design award winning products. Recently JW Winco’s GN 328 and 428 Cabinet U-Handles and the GN 126 / GN 126.1 were awarded the European iF DESIGN AWARD. GN 328 and GN 428 Cabinet "U" Handles Aluminum, are recognized for their stability, and ergonomic grip, these handles are made from solid aluminum and reflect the latest developments in industrial design. The GN 126 and GN 126.1 flat adjustable tension levers are characterized by their low height and are an ideal choice whenever swiveling in a confined space is required. The sophisticated function of the serrated teeth enables smooth engagement and adjustment of the flat tension lever.

Visit JW Winco at the WestPack show in Anaheim, California booth #5130 to see our products mentioned above and our full range of standard parts!
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
Für diese Landesversion verlassen Sie die aktuelle Webseite und werden zur jeweiligen Landesvertretung weitergeleitet. Bitte beachten Sie, dass es zu Abweichungen von Darstellung und Inhalten kommen kann.

Sie werden nicht automatisch weitergeleitet. Bitte klicken Sie den unten genannten Link.

Note about forwarding

For this country version you leave the current website and are forwarded to the respective country representation. Please note that there may be deviations in presentation and content.