JW Winco is exhibiting at the NAMM (National Association of Music Merchants) 2019 Show!

NAMM-Winco-parts

Handles, Knobs, Clamping Levers, Anti Vibration Mounts, Leveling Devices and other Components are used on products in the music, sound, light, event and stage design industry. JW Winco has many different metric and inch standard parts for your unique applications.

JW Winco has been helping companies find the perfect part for their application need for over 40 years. Below are some examples of the parts & hardware that JW Winco has supplied to companies exhibiting at the NAMM show and in similar industries.

JW Winco’s Adjustable Levers and Knobs have been used as accessories in many different musical instrument and microphone stands. Our WN 300 Plastic Adjustable Lever is ideal when an application requires clamping in a confined space, typically used on drum sets and cymbal stands. Our Indexing Plungers like the GN 822.1 Mini Indexing Plungers are used for locking multiple studio speakers in place as well as holding studio lights in a fixed location.

JW Winco’s knobs like the GN 6336 series Star Knobs have been used for adjusting production lighting and are used on equipment carts for theaters, studios, motion picture, television, video and photography. Our MF Series U-Handles are also used for pushing and controlling the movement of the carts and road cases. These types of carts and road cases are primarily used by grips and gaffer for lighting, rigging and electrical.

Other components that JW Winco supplies that have been used is the music, stage and lighting industry are the WN 9100 & LPST "LEVEL-IT"™ Leveling Mounts. The leveling mounts are suitable for light, medium, and heavy-duty applications. JW Winco's new GN 784 Mounting Clamps with Swivel Ball Joint combined with the GN 51.3 Retaining Magnets with a shortened stud would be the ideal for holding lights & cameras that require quick adjusting. 

Visit JW Winco at the NAMM show in booth #12141 in Hall A to see our of our products mentioned above and our full range of standard parts!

JW Winco's WN 100.1 and RP 200 quick release pins could also be used as replacement pins for JBL speakers and speaker arrays depending on the size. To request replacement pins that are manufactured to JBL specifications please refer to our JBL Pins Product Page. 
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
Für diese Landesversion verlassen Sie die aktuelle Webseite und werden zur jeweiligen Landesvertretung weitergeleitet. Bitte beachten Sie, dass es zu Abweichungen von Darstellung und Inhalten kommen kann.

Sie werden nicht automatisch weitergeleitet. Bitte klicken Sie den untern genannten Link.

Note about forwarding

For this country version you leave the current website and are forwarded to the respective country representation. Please note that there may be deviations in presentation and content.