JW Winco now offers Inch Size Steel and Stainless Steel Gear Lever Handles

GN-310-Inch-Size-Gear-Levers

JW Winco announced it has expanded its line of GN 310 Steel and Stainless Steel Gear Lever Handles to a full range of inch and metric sizes.

JW Winco, Inc., A Ganter Company, a leading supplier of standard industrial machine components, now offers GN 310 Steel and Stainless Steel Gear Lever Handles, available in inch as well as, metric sizes.

      Both versions of the Gear Lever Handles are RoHS compliant. The steel lever option is zinc plated with a blue passivated finish and there is a variety of operating knobs to choose from dependent on their function and/or their design. The stainless steel version has a sandblasted satin finish and is an excellent choice for applications requiring corrosion free environments. The knobs on both are black Duroplast (Phenolic PF) with a shiny finish and have a maximum heat resistance of 150°C (300°F).

Back

JW Winco Press Releases

Click below for press releases on new products or additions and extensions to our product range!

Go to the Press Releases

New Products

Click below to hear about our new products or new additions to our product range!

Go to New Products