Steel Control Levers Now Available from JW Winco

Control Levers

New GN 223 Steel Control Levers perform smoothly and powerfully thanks to the heavy-duty arm of the lever.

JW Winco, Inc., A Ganter Company, a leading supplier of standard industrial machine components, announced it has available GN 223 Steel Control Levers with Round Through Bore, with or without Keyway and Square Through Bore versions.

      These RoHS compliant control levers, offered standard in metric sizes, feature a steel hub and arm with a black oxide finish, while the ball knob is black phenolic plastic with a glossy finish. Inch size Bores, Keyways, Set Screw Holes are available upon request.

      The GN 223 Steel Control Levers perform smoothly and powerfully thanks to the heavy-duty arm of the lever.

      JW Winco offers an extensive selection of inch and metric size adjustable levers, cabinet U-handles, plastic and steel hinges and locking mechanisms, revolving and retractable handles, hand wheels, hand cranks, tube connection and conveyor components, inch and metric construction tubing, shock absorption mounts, leveling mounts, hand knobs, spring, ball and indexing plungers, jig, fixture and fastening components, retaining magnet assemblies, toggle clamps, metric casters and wheels, universal joints, oil sight glasses, and metric tools for the industrial and commercial equipment industries. JW Winco’s new website, with improved 3D CAD and online buying, is viewable at www.jwwinco.com.

      JW Winco, which is ISO 9001:2008 certified, is located in New Berlin, Wisconsin, with sales locations in Canada and Mexico. For more information, contact JW Winco at 800-877-8351, by fax at 800-472-0670, on the Web at www.jwwinco.com, and via e-mail at sales@jwwinco.com.

Back

JW Winco Press Releases

Click below for press releases on new products or additions and extensions to our product range!

Go to the Press Releases

New Products

Click below to hear about our new products or new additions to our product range!

Go to New Products