JW Winco, Inc., A Ganter Company, a leading supplier of standard industrial machine components, has recently introduced WN-913.3 Inch Size Steel Set Screws, with Brass or Nylon Tip.
These set screws, with a black oxide finish, are used primarily in applications where you want to avoid the marring of a shaft or damaging a soft piece of material, but still need to secure it in place with the brass or nylon tipped set screw. They can be used with a variety of different parts, including levers, hand knobs, star knobs, and knurled nuts.
“Those that operate in the area of machine building, including medical, packaging, and pharmaceutical, and material machining would find these set screws work very well for applications within these industries,” said John Winkler, CEO, Office of the President at JW Winco.
For the Metric set screws see the GN 913.3.
AtrásComenzando el 15 de junio de 2024, implementaremos un ajuste de precios. Algunas piezas tendrán una disminución en su precio mientras que otras tendrán un aumento. Estos ajustes nos ayudan a asegurar nuestro compromiso de proveer a nuestros clientes con los mejores productos y servicios.
Respetaremos los precios publicados actualmente hasta el 14 de junio de 2024.
Gracias,
J.W. Winco