JW Winco, Inc., A Ganter Company, a leading supplier of standard industrial machine components, now has available an expanded range of Rod End Bearings, including GN 648.1/GN 648.2 Steel Zinc-Plated, Tapped Type or with Threaded Stem and GN 648.5/GN 648.6 Stainless Steel, Tapped Type or with Threaded Stem.
The GN 648.1 and the GN 648.2 zinc plated steel rod end bearings housing’s have a blue passivated finish. For the pairings, the bearing socket on the version where lubrication is possible is brass, while the self-lubricated version is steel, zinc plated. The internal ring for both is steel, hardened, ground, and polished.
The GN 648.5 and the GN 648.6 bearings have a stainless steel housing that is forged and polished. For the pairings, the version with the lubrication fitting features a bronze bearing socket with a steel internal ring that is hardened, ground, polished, and hard chrome plated. The two self-lubricated versions have pairings with a PTFE-insert, with one made of bronze and the other of stainless steel, with an internal ring that is also stainless steel
Rod end bearing are also known as a heim joint or rose joint or ball joint heads. Rod end bearing are a mechanical articulating joint that transmit traction and thrust from linkages and lever arms. Rod end bearing are used on the ends of control rods, steering links and tie rods.
AtrásComenzando el 15 de junio de 2024, implementaremos un ajuste de precios. Algunas piezas tendrán una disminución en su precio mientras que otras tendrán un aumento. Estos ajustes nos ayudan a asegurar nuestro compromiso de proveer a nuestros clientes con los mejores productos y servicios.
Respetaremos los precios publicados actualmente hasta el 14 de junio de 2024.
Gracias,
J.W. Winco