JW Winco, Inc., A Ganter Company, a leading supplier of standard industrial machine components, now offers GN 4490 Zinc Die-Cast Ball Catches.
JW Winco’s GN 4490 ball catches are used, for example, to hold flaps and doors closed that must be opened and closed frequently and easily. They consist of a ball housing and a retaining element that engages in the ball housing from the side or front. The installation orientation can be chosen as desired.
“Beyond the typical uses, these solid and attractively designed ball catches are utilized in in a variety of applications,” said John M. Winkler, CEO, Office of the President at JW Winco. “Due to the centered 90° countersunk holes, they can also be used with aluminum t-slot profile systems as a door latching mechanism.”
The ball catches are powder coated in either black or silver and have a textured finish, the ball and spring are stainless steel, while the ball guide is plastic.
AtrásComenzando el 15 de junio de 2024, implementaremos un ajuste de precios. Algunas piezas tendrán una disminución en su precio mientras que otras tendrán un aumento. Estos ajustes nos ayudan a asegurar nuestro compromiso de proveer a nuestros clientes con los mejores productos y servicios.
Respetaremos los precios publicados actualmente hasta el 14 de junio de 2024.
Gracias,
J.W. Winco