Load rings and lifting points are extremely strong, reliable parts for safely lifting, lowering or lashing down heavy loads. They can be welded on as a permanent attachment or can be removeable by using screws.
Depending on the requirement, the user can choose between fixed or rigid lifting points and mobile lifting gear that can be either rotated or folded.
There are two types of lifting points:
The load rings (also called swivel hooks) and load rings offer many features:
The freely rotating hook or ring on a ball bearing prevents tension in the rope or chain while carrying the load or when turning parts. The safety latch on the hook prevents the crane hook from slipping even when relaxed. The integrated RFID chip simplifies identification for regular inspections.
Attention Valued Customer,
Beginning February 16, 2026, we will implement a price adjustment. Some items will have a price decrease, while others will increase. The adjustment helps ensure our commitment to providing our customers with the best products and services.
We will honor current published prices through February 15, 2026.
Customers with pricing agreements will not be affected until annual pricing is reviewed.