Pulling Force Information for Retaining Magnet Assemblies

Other factors aside from the magnet material and the size of the magnet affecting the magnetic pulling force are:

The magnetic pulling force can also be impaired by alternating thermal stress and by chemical factors (aggressive baths, gases, etc.).

The diagrams and graphs below show guide values relating to the impact on the magnetic pulling force caused by different mechanical specifications.

The nominal magnetic pulling forces shown in the tables of the standard pages are minimum values which are achieved at:

Force Measure

1 Newton (N = .225 lbs.)